STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 variable not updating in interrupt handler

Hello,i have a strange situation happening and I really can't catch the reasons; in my project I set up an SPI transfer and set a global volatile variable that keeps trace of status state://Transmit Data if(spi == AMPLI_SPI4) SPI4_TransferState = TRA...

MSard by Associate II
  • 3625 Views
  • 6 replies
  • 0 kudos

FreeRTOS : Inerrupts

I work with FreeRTOS and I have two interrupts that can be triggered at the same time: An interrupt on a Timer in Input Capture mode (because I'm working with an ultrasound sensor HCSR04) and a UART interrupt (which is the reception of 'a character )...

AGHAZ by Associate II
  • 2515 Views
  • 5 replies
  • 0 kudos

pdf library

i have found a library https://github.com/Jun1172/stm32_pdflib_msc_storagebut it need much ram and ZI DATA 14k about pdf,so i want to know is there a small libray

How to check if ROM is okay on STM32F030

ROM Check on STM32F030I have an STM32F030 where my product has a requirement to do a ROM check before performing any task. How can I do it? Is there any API which returns the result of ROM check done in bootloader? What’s the easiest way of achieving...

Resolved! Please advise plans to upgrade CubeMX to LWIP 2.0.3

Posted on October 25, 2017 at 10:48The latest version of CubeMX 4.23 is still at LWIP 2.0.0However on the LWIP site they note in bold:from http://savannah.nongnu.org/projects/lwip/ All users using 2.0.x are strongly suggested to upgrade! I'm particu...

CubeMxIDE v1.0.2 for STM32f031x6 ADC usage problem

I am using CubeMxIDE v1.0.2 with STM32f031F6Tring to read internal batt and temperature. But can not successfull.. I found that SMT32F031x6.h library file and corrected the following lines#define ADC_CCR_VREFEN_Pos       (22U)                        ...

istepne by Associate III
  • 738 Views
  • 1 replies
  • 0 kudos