cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-L476RG as USB FS serial device

MSuhe
Associate III

Is the CN1 USB Mini-B connector on the NUCLEO-L476RG board also connected to the STM32L476 target? Or it is only for ST-LINK-V2-1 section.

If the CN1 connector is only for ST-LINK-V2-1 then one has to solder a USB socket to the STM32L476 target to use it as USB FS device?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

See also, in case you're related https://community.st.com/s/question/0D50X0000A1n3jISQQ/unable-to-establish-nucleo-stm32l476rg-usb-cdc-communication

The schematic should be pretty clear on this, pull the manual and review if you haven't done so.

The mini-USB connects only to the F1 part providing ST-LINK functionality. You'll need to manually wire USB connectivity to the L4. Perhaps consider an Nucleo-144 board that has two USB, one connected to the target.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for your response. I am planning to hay-wire a USB mini-B connector to the relevant IO lines on the ST morpho connector. So that i can use the USB port on STM32L4 target.

Is there a schematic that i use here for reference. I am aware of the USB pinout and should be able to hay-wire the connector. But, just wanted to know if i need to have any diodes etc in the circuit for protection.

Thanks.