STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IAP_Main cannot receive via ymodem

I am trying IAP using a new sample application for the STM32H753I-EVAL2 board. STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/Applications/IAP/IAP_MainIAP_Main would download IAP_Binary_Template image into flash memory. However, IAP_Main can tran...

chuan_lee by Associate II
  • 1181 Views
  • 1 replies
  • 0 kudos

USB_OTG_FS registers similar to USB_OTG_HS ?

hi, I want to use USB-FS. For initialisation I used the tool integrated in the cube IDE. The RM contains the HS-registers but not the FS-registers. Since the tool changes bits that are not supposed to be changed (namely: GOTGCTL) I assume the registe...

Incorrect DMA transfer when address isn't aligned.

Hi,We using the HAL_ADC_Start_DMA() function and this function works very fine when the pData pointer is aligned to 4. (data transfer is DMA_PDATAALIGN_WORD)Unaligned data can be happen when the *pData is defined as a structure and the structure is p...

OGhis by Senior
  • 875 Views
  • 0 replies
  • 0 kudos