STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DHCP does not work when I change my Mac Address.

 Board: STM32746G-DiscoveryProject: LwIP_HTTP_Server_Netconn_RTOSPosition: ethernetif.c stm32f7xx_hal_conf.h#define MAC_ADDR0  0U#define MAC_ADDR1  2U#define MAC_ADDR2  0U#define MAC_ADDR3  0U#define MAC_ADDR4  0U#define MAC_ADDR5  0UWhen set as abov...

Bootloader behavior

Hi,I need some help to understand the behavior of the bootloader.Currently I use STM32F746 but I will move to STM32F778AI next week.I have several needs from bootloader:Load bootloader if there is no user application.Load user application on start ( ...

davidra7 by Associate II
  • 766 Views
  • 3 replies
  • 0 kudos

Resolved! Where are the DEMO source project file for the OUT OF BOX demo for the Nucleo-64 STM32F303RE board.

I purchased a Nucleo-64 STM32F303RE for beginning a project. I have downloaded the tools, this includes CUBE_MX and CUBE_IDE. I am able to build a project using these tools as instructed. What I want to know is where is the DEMO project that is loade...

TFlac by Associate III
  • 886 Views
  • 2 replies
  • 0 kudos

How to restart into bootloader (with DFU).

typedef void resetvec(void);       void cmd_jbl(BaseSequentialStream *chp, int argc, char **argv) // reboot to bootloader   {    unsigned int t;        (void)argc;     (void)argv;    (void)chp;    resetvec *fun;         fun = ((uint32_t *)0x1fffc800)...

UCB CVP won't work in STM32F412RG

I'm struggling already many days getting the most simple VCP functionality working in my application.I tried implementing the UM1021 usb OTG lib provide as extension on the STD peripheral library from ST, but without succes. After that I tried the s...

SMaes.3 by Associate
  • 529 Views
  • 0 replies
  • 0 kudos

Hello! I'm testing FatFS on my evaluation board and is working only for a 2gb sd card. I'm using the example from the Cube repository. Can anyone help me?

I'm need to use a microSD card on my new project, so I decided to test in my evaluation boards. I have a STM32373C-EVAL and a STM3210C-EVAL boards. For the tests I used 2Gb, 4Gb, 8Gb and 16Gb sd cards. Now came the problem, on the STM32373C-EVAL only...

What is the difference between 'USB CDC' and 'USB HID'?

I'm using STM32F072VB.​I want to communicate with 'USB' instead of 'Serial'.Should i use ​'USB CDC(VCP)'? or Should i use 'USB HID'?I ​created a 'USB HID' test code with CubeMX and checked it. ( Reference Image1)​​<Image1>​Can i do 'download communic...

0690X0000098Qi7QAE.png
LHAEU by Associate
  • 1348 Views
  • 0 replies
  • 0 kudos