STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL CubeMX I2C slave NACK problem (STM32F446)

Technical environment :-       Master : CM3 (Raspberry)-       Slave : STM32F446-       CubeMX : V4.23 (even tested with V4.26.1)-       Normal transaction is : MASTER do a 4 bytes WRITE, then a 1 byte WRITE and at last, a 4 bytes READ.The slave ACKe...

0690X000006By7MQAS.png
YBOUR by Associate II
  • 4309 Views
  • 6 replies
  • 0 kudos

system boot loader FDCAN

Rev V system boot loader FDCANSTM introduces boot via FDCAN1 with chip revision V.The system boot loader version ischanged form V13.3 to V9.0. I’ve tried to figure out how does it work. Here are my findings-     AN2606 rev 38 is updated. It describes...

MMagl by Associate III
  • 2237 Views
  • 3 replies
  • 0 kudos

STM32F4 Read wav from USB

Hello everyone! I'm working on a project like Audio Playback. I have tried compile and run Audio_playback_and_record from ST's Firmware pack its working good.I'm trying create my own project file, i'm stuck in read wave data from usb. I can get wavef...

0690X00000AtQ57QAF.jpg 0690X00000AtQ5CQAV.jpg
emetians by Associate II
  • 4404 Views
  • 8 replies
  • 0 kudos

Resolved! STML432KC: CAN Bootloader functionality

Refer to AN2606 p. 260 - 263There it says, that for STM32L43xxx derivatives CAN1 bootloader is mapped to PB8 pin (RX) and PB9 pin (TX). My derivative supports CAN but doesn't have these pins, because of a 32 Pin package. Is there a possibility to use...