STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STML432KC: CAN Bootloader functionality

Refer to AN2606 p. 260 - 263There it says, that for STM32L43xxx derivatives CAN1 bootloader is mapped to PB8 pin (RX) and PB9 pin (TX). My derivative supports CAN but doesn't have these pins, because of a 32 Pin package. Is there a possibility to use...

Resolved! USB port for debug and programming

Hello,I've been using the NUCLEO-L476RG board for development. Now I want to design my own PCB with the same component. My question is about the JTAG port - in the NUCLEO board it is implemented as a USB connector but they used an additional uC for t...

Resolved! ADC DMA and interrupt

Hey.Im using adc dma to transfer data from adc to memory. After each sequence of conversion I need an interrupt.My first question is that is using dma in my case something useless?My second question is that after adc sequence of conversion interrupt ...

Cannot get USB VPC to work, bootloader / DFU mode works

Hi All,I have a strange problem. I made a custom board with a stm32l151VETx and i cannot get the VPC to work. No device shows up in the device manager nor on linux under dmesg. However if I change the boot pins so that the internal bootloader starts ...

0690X00000AtPJmQAN.png
mmj by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

STM32F107 FreeRTOS+NetConn won't work

Hello.I'm trying to stitch-up the STM3210C LwIP TCP/IP Echo client example (my board) and STM324xG LwIP+FreeRTOS+NetConn example.LwIP, and netif config are the same as for Echo example (and previously I ran httpd-raw server with it).I was able to set...

zedeg by Associate III
  • 800 Views
  • 0 replies
  • 0 kudos