STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RS485 Receive DMA lock and busy randomly

Hello,I'm doing Modbus communication using RS485. And using MAX485 IC to convert to RS485. and running on Free RTOS CMSIS.I have tried and the behavior is random for all below, not consistent. Here I have tried with RS232 and it works like charm. The...

hdmarx_lock_busy_error.jpg

UART3 overrun interrupt

Hello,It is the first time I am using STM32 and migrating my code from texas instruments controller using USART3. I want to receive data and then transmit data of different sizes. I get a problem that I see appears often but in my case I cannot see w...

GTanova by Associate III
  • 2061 Views
  • 15 replies
  • 13 kudos

Ethernet Request time out issue

  Hello everyone, I am working with an STM32H5 series board and have successfully initialized Ethernet using the lwIP stack.The DHCP process works correctly — I am able to obtain an IP address. However, I am facing a “Request Timeout” issue when I tr...

Resolved! UART output is garbled on Tera Term

I ran the example project and successfully displayed “Hello World” on Tera Term.Then I tried to port this project into my own one.However, the result was garbled characters in the terminal.The baud rate (115200) and PLL/clock configuration are the sa...

chachamaru_0-1762764753839.png chachamaru_1-1762764754652.png chachamaru_2-1762764753839.png chachamaru_3-1762764753837.png

USB microphone from the USB speaker example

Hi,Tried to convert STM32CubeN6\Projects\STM32N6570-DK\Applications\USBX\Ux_Device_Audio_2.0 example of the USB speaker to the USB microphone on STM32N6570-DK.The USB device is enumerated as an audio recording device, ux_device_class_audio_stream_fra...

ERROR by Senior
  • 436 Views
  • 1 replies
  • 0 kudos