STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Package for STM32F1 Series 1.8.0 trouble

Use this "STM32Cube Package for STM32F1 Series 1.8.0" ,  This statement:__HAL_TIM_SET_CAPTUREPOLARITY(htim,TIM_CHANNEL_2,TIM_INPUTCHANNELPOLARITY_FALLING); is wrong.   Tips: ../Src/freertos.c(417): error: #53: expected a ":"but in 1.7.0, it is Correc...

lzai by Associate
  • 2705 Views
  • 4 replies
  • 0 kudos

PWM DMA: Interrupt Callback not working on STM32L452

Sorry if the question sounds stupid, I am new to STM32.I managed to have a PWM working, timer 1, pos/negative, deadtime, working with DMA from an array with pre-calculated values. HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, sine_val, samples); HAL_T...

maelli by Associate II
  • 635 Views
  • 0 replies
  • 0 kudos

How to activate debug messages for LWIP?

I was able to activate the messages for USB Host, but I am not able for LWIP, it seems that there is a specific combination of options, so that messages are enabledThank you./** Enable debug message printing, but only if debug message type is enabled...

0690X00000DYNnfQAH.png
by Not applicable
  • 6088 Views
  • 1 replies
  • 2 kudos

HAL_SMBUS drivers for STM32L0

Hello,I am trying to use HAL_SMBUS drivers on STM32L0. The STM32L0 is the slave and I want to read / write registers via i2cget and i2cset on the linux host. I do not need the full SMBus/PMBus middleware, just looking for a simple example with SMBUS ...

Do I can reproduce sound with L031E?

Hi, I need choose a STM32L0 microcontroller for reproduce sound, I had thought choose L031E because is smaller and it have few GPIO, but I don't know if I can reproduce sound whit it. I don't need many GPIO, that's way I though about it.Caracteristic...

Melxo by Associate II
  • 1630 Views
  • 2 replies
  • 0 kudos