cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USB-PD Power Delivery Software Expansion

FaikN
Associate II

Hey,

I am working on one of the example projects that is provided as part of USB-PD software expansion, by using SW4STM32 toolchain. I am using TCPM-TCPC architecture. During initialisation i am having errors for PE_Init. Does anyone have followed a similar topology and can help me on how to tackle with this problem? Thanks.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Yohann M.
ST Employee

Hello

Could you please precise the version of the expansion package you are using?

Do you just have an error of PE_Init or is it a timeout to initialize the TCPC component?

Normal stack calling of expansion package STM32CubeExpansion_USBPD_F0_V2.1.0:

HAL_I2C_Mem_Read() at stm32f0xx_hal_i2c.c:1 884 0x800985c

USBPD_TCPCI_ReadRegister() at usbpd_tcpci.c:606 0x8008f9e

fusb305_tcpc_get_power_status() at fusb305.c:909 0x800801c

fusb305_tcpc_init() at fusb305.c:326 0x8008166

USBPD_PHY_Init() at 0x8005b50

USBPD_PRL_Init() at 0x8004d82

USBPD_PE_Init() at 0x8000186

USBPD_DPM_Init() at usbpd_dpm_core.c:292 0x8009c40

main() at main.c:83 0x8007320

Regards,

Yohann

FaikN
Associate II

Hey Yohann,

I have fixed the problem. I have been using F0.V2.1.0; it was actually during the initialisation of TCPC component. now fixed. Indeed thanks for your response. I will contact promptly if there are other issues. Regards,

Faik

FaikN
Associate II

hey Yohann,

I have recently a USPD_MALLOCERROR from the initialisation function of USBPD_TCPM_HWInit function; that initialises the TCPC. What can be the reason for the malloc error in this function? and what can be the solutions?

Thanks,

Faik