I am using standard peripheral library and OTG FS core in FS host only mode just talking about connection , not enumeration. When the hub is not connected I never see the PCDET bit in HPRT register set
Hello folksThis is my first time working on ST processor and USB and need some help I am using STM32F407VG Processor in the host only mode and standard peripheral libraryI am not using SOF and using HSE as an input to the PLL operating at 168 MHz I e...