STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB Host HID mouse

Hi, I'm developing an application using a custom board based on STM32F429BI.Here is my setup/configurations- STM32 CubeMX 1.1.0 to generate code initialization.- Using USB_HS port configure as HOST- Using STM32 HID Host Driver- Using FreeRTOS- Using ...

0693W000000UYEHQA4.png

Connect to HTTP to download file

Hello,I'm using STM32H753I-EVAL, and I want to connect to HTTP web service, to download files.There are a lot of examples to set the STM32 as server, but I want the opposite way. I want to my STM32 will be connect to external (via Ethernet) HTTP serv...

Lmali.1 by Associate III
  • 1474 Views
  • 1 replies
  • 0 kudos

FATFS SDIO Stability issue

Packages DetailsSTM32F446RE NucleoCubeMX 5.6.0STM32CubeF4 Firmware Package V1.25.0 / 12-February-2020if i write every 30ms 512 Bytes. After some time SD card takes more time then normal please check image.GPIO Pin Set before writing and Reset after w...

0693W000000UTDOQA4.png
Jutt by Associate II
  • 818 Views
  • 0 replies
  • 0 kudos