USB CDC device sometimes fails to receive
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-25 1:40 AM
I'm using the USB CDC library on a STM32L452 created with CubeMX and have run into some problems with receiving data over USB. Every week or so I experience that the device stops receiving data (the transmit side works fine). In other words, the CDC_Receive_FS callback function is not triggered when I try to send data? Inside the CDC_Receive_FS there is a call to USBD_CDC_ReceivePacket which is preparing the OUT endpoint for reception. But since CDC_Receive_FS is not called, the OUT endpoint will never be ready to receive the next packet. When the problem occurs, I have tried to "manually" call the USBD_CDC_ReceivePacket which indeed makes the device start receiving data again.
So my questions are:
- Why does this happen?
- Are there any fixes?
- Are there anything I can do to detect when it has happened so that I can call USBD_CDC_ReceivePacket to bring the receiving side back?
Best Regards,
/abaldur
- Labels:
-
STM32L4 Series
-
USB