Skip to main content
SSin
Associate II
April 25, 2019
Question

FreeRTOS + GPIO won't work after naming GPIO

  • April 25, 2019
  • 0 replies
  • 376 views

Hi all,

I made a PCB with STM32F103RE. And I build a code with STM32CubeMX, which contain FreeRTOS, a GPIO input & a GPIO output. I can write a program that flash a LED driven by the output GPIO. But once I rename the GPIOs via STM32CubeMX, the LED can't flash again. Even I removed the name, it still can't flash. It is 100% repeatable. Can anyone tell me what have I did wrong & how can I recover?

My environment is as below:

OS: Windows 10

STM32F103RE version: 5.1.0

IDE: Visual Studio Code (ver 1.33.1)

GCC version: 7.3.1

Attached please find my project

This topic has been closed for replies.