STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 USB MSD Bootloader can't connect to WIN10.

This is the second time I’ve asked for help about coding a USB MSD bootloader for the STM32L4 using the STM32L4R9I-EVAL board. I gave up for a while but would really like to figure this out so I can move forward and be able to use the STM32L4. I used...

erussell by Associate II
  • 631 Views
  • 0 replies
  • 0 kudos

unrecognized usb driver in windows

Hello Im using STM32F407VET6 and im having a problem with the USB driver with the windows, when i plug the usb, the operational system dont recognize the microcontroler and shows me this error: unrecognized usb driver. I already installed the driver ...

TIM macros

My programming level is initial. Breaks with STM32L432KC.I would like to use the dynamic change of the TIMx period as soon as the TIMx Interruption from the previous period. How to practically use the _HAL_TIM_SET_AUTOREOLAD macro to load a new value...

CJaro by Associate
  • 671 Views
  • 1 replies
  • 0 kudos

Resolved! UCPD sink with external pull-down resistors?

Hey,the STM32G431 data sheet states that the UCPD unit has internal pull-down resistors. Now I want to flash my G431 via DFU, and USB-C doesn't provide power to a sink unless CC1 and CC2 are pulled down. It seems that the internal UCPD only works whe...

nicolai86 by Associate II
  • 2628 Views
  • 6 replies
  • 0 kudos

!!! BUG FOUND !!! : New Firmware version 1.8 introduced a sort of bug in USB Host enumeration - tested with STM32F105

If you upgrade to the last firmware (1.8) it will make the USB enumeration process no more work.To repeat the process just create a project using USB and put a breakpoint at the lines for each eventstatic void USBH_UserProcess (USBH_HandleTypeDef *p...

MAlek by Associate II
  • 1738 Views
  • 7 replies
  • 0 kudos

STM32L496 dual bank boot difficulty

I can't figure out how to get the STM32L496 to boot at all with BFB2 set to 1.Using nBoot0_SW_Cfg=0 and nBoot0=1,With BFB2=0, I can boot successfully from bank 1With BFB2=0, I can copy the contents of bank 1 to bank 2 and swap banks using the FB_MODE...

Resolved! I have recognition problem with NUCLEO G070RB

I start working with the Nucleo board G070RB and I’m new with ST products. I follow the instruction of the user manual but my board isn’t recognised by the UCPD Cube monitor and the USB STLINK LED is red. Otherwise, it is recognised by my computer. C...