STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TCP Server & Client, lwIP Netconn API

Dear friends, I am trying to establish a robust TCP interaction between two different boards with the same MCU (stm32f407vgt6) and ethernet phy (dp83848cvv) and I use lwIP Netconn APIs as TCP/IP stack and freeRTOS as a real time operating system.In b...

Mujtaba by Senior
  • 5166 Views
  • 2 replies
  • 0 kudos

Connection forcibly closed by the remote host!

Dear friends,I am working on a TCP Server taks running on STM32f407VGt6 MCU and NetConn APIs.Sometimes when a Client tries to connect to the Server, the Connection is closed by the Server and the error is Connection forcibly closed by the remote hos...

Mujtaba by Senior
  • 954 Views
  • 0 replies
  • 0 kudos

STM32 delay not working as expected with USB HID

I am trying to send a shift + U keypress to the screen every two seconds but it is just printing U's nonstop. Why isn't it delaying for two seconds? How do I properly debug stuff like this in the future? while (1) { hid_report_buffer[0] = 0x02;...

JMora.2 by Associate II
  • 1077 Views
  • 2 replies
  • 0 kudos

STM32F103CB not entering the bootloader...

Hi, I am making a custom PCB. I am able to reliably flash it with a ST-Link and a Segger programmer. I also have a custom program that I use to flash the MCU using the UART. It has worked for years with other ST chips and partially worked with th...

PhilSter by Associate II
  • 2736 Views
  • 5 replies
  • 0 kudos

What is the right way of porting amazon freertos?

Hello,I tried the poritng guide but it took forever to fix the missing and conflicting paths, and it's not clear what to compile and what not to.I want to have mqtt + lwip + mbedtls + PPPOS (I can start with Ethernet as a start).I can use other SDKs ...

AWahd.1 by Associate II
  • 848 Views
  • 0 replies
  • 0 kudos

FreeRTOS on STM32

I am new to ST Micro development boards and environment and want to learn FreeRTOS on STM boards. Which board should I buy to start with? Does ST micro provide development boards as a sample to learn ?Thank you,Prachi Patil

PPati.4 by Associate
  • 1395 Views
  • 2 replies
  • 0 kudos

Resolved! BSP_AUDIO_OUT_Play ends up in Default_Handler

Hello,I try to play a sound using stm32h747i_discovery_audio.c. Initialization goes well void CAudioController::AudioOutInit() { BSP_AUDIO_Init_t audioOutInit;   if (!audioOutInitDone_) { audioOutInit.Device = AUDIO_OUT_DEVICE_HEA...

ALevc.1 by Associate III
  • 1866 Views
  • 2 replies
  • 0 kudos