Skip to main content
JLojo
Associate III
June 6, 2019
Question

Is VCP diver able to handle several devices on Windows 10?

  • June 6, 2019
  • 4 replies
  • 756 views

Hello,

I'm using VCP to communicate with an STM32F303 device, which works well.

However, when I plug a second device on the same computer, it fails to enumerate properly with the message 'This device cannot start. (Code 10)'.

Is that a known issue?

Is there a way to connect several STM32 on the same computer?

Thanks

jyl

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
June 6, 2019

And if you unplug the first device and plug in the second one?

Don't they draw excessive power?

JW

JLojo
JLojoAuthor
Associate III
June 6, 2019

Both work perfectly as long as they are alone on the computer...

jyl

Pavel A.
June 6, 2019

Non unique "serial number" ?

-- pa

JLojo
JLojoAuthor
Associate III
June 6, 2019

Hmm, maybe same ID...

I thought serial number was assigned automatically for each device...

I'll check this in mode details.

Thanks Pavel!