STM32F105 USB problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-10 12:34 AM
I use a STM32F105. On the board there is a bootloader and I upload the firmware through USB (host, OTG_FS). Then I use the USB to extract a log file (.txt). The extraction of the log works only if the optimization of the code is 0. If I set optimization 1, 2 or 3 micro restarts while USB is inserted for the log extraction. I need to make it work at least with optimization 1. The strange thing is that if I upload the firmware without bootloader on the board, it works also with optimization 3.
Labels:
- Labels:
-
STM32F1 Series
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0