STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have a question about hid otg connector selection

I am trying to implement hid otg with stm32f105But you can use micro 5pin as otg usb connectorUSB communication does not work with the normal connector as shown in the picture below.I wonder why it doesn't work depending on the usb connectorAnd is th...

0693W000001cOPjQAM.jpg
HSHIN.1 by Associate
  • 1408 Views
  • 3 replies
  • 0 kudos

STM32 USB Data Logger

Which Software you are using to monitor the Receive and transmit data from USB. Do you have any suggestions for the USB data Loggers ?

Smalik by Associate II
  • 723 Views
  • 0 replies
  • 0 kudos

USB Audio issues with repeat INCOMPISOOUT interrupt

I'm having trouble implementing the Audio Device Class example from the STM32CubeMX tool on a STM32H750VBT6. When run, the USB appears to enumerate properly, installs the default drivers (Windows 7, btw) and shows up properly as a playback device. Ho...

YDong.11 by Associate II
  • 928 Views
  • 0 replies
  • 0 kudos

BSP_AUDIO_OUT_Play

I wonder what is a best way to play a file in small chunks? Is there is a standart way of doing it or you should make a timer that expires just before the previous data is played and then call BSP_AUDIO_OUT_Play() again?

ALevc.1 by Associate III
  • 1237 Views
  • 1 replies
  • 0 kudos