STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I determine Source PDO capabilities?

I am developing an application using an STUSB4500 and an external MCU STM32G031K8 that should be able to read USB PD Source capabilities and allow the user to dynamically set custom PDOs.I have based the majority of my code off of the example softwar...

ardnew by Associate III
  • 1597 Views
  • 2 replies
  • 0 kudos

Using X-Cube-Azure IoT kit P-L96G-CELL01 with UG96 Cellular Modem. The push button switch is not recognized so I cannot enter cellular credentials or TLS root CA certificate. Using software version 1.2.0. Tried pressing blue (joystick) during …...

Tera Term log:Starting Main Thread...****************************************************************  HWJ AZURE***  STM32 IoT Discovery kit for***     STM32F413/STM32F769/STM32L475/STM32L496 MCU***  X-CUBE-AZURE Cloud Connectivity Demonstration***  ...

Name & description of HAL_GetTickFreq() misleading?

From the function name of 'HAL_GetTickFreq()' function, I expect that it returns tick frequency in Hz.But I experienced that it returns tick period in milliseconds. If tick frequency is 1000 Hz, then it returns 1, that value comes from HAL_TICK_FREQ_...

Lazac by Associate
  • 1188 Views
  • 0 replies
  • 2 kudos

STMH755 and FDCAN Bootloader settings

Hi,I've been going through application note AN2606 for the bootloader in STM32H755.The note says that pattern 10 needs to be executed.Pattern 10 has two conditions:Boot(pin) = 0 and BOOT_ADD0(optionbyte) = 0x1FF0Boot(pin) = 1 and BOOT_ADD1(optionbyte...

TOlli by Senior
  • 685 Views
  • 0 replies
  • 0 kudos

Code example request to ST: USB HID keyboard

Hello,I just wanted to ask for a code example (middleware) for a USB HID keyboard. Currently, there is only a mouse / joystick available. (The situation has not changed from this discussion 3 years back: https://community.st.com/s/question/0D50X00009...