STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using USB hub with STM32F7 USB HS

Hello,I'm designing an embedded system that connects to a PC for USB data and converts it to an analog signal.This is an HS USB device with 2 USB ports which needs to process 4 channel 40Mbps data.This device can work as a single system, but with som...

0690X00000BvotTQAR.png
BHan.1 by Associate II
  • 2096 Views
  • 12 replies
  • 0 kudos

Resolved! Whats the use of System memory & flash memory

Please any one help how to differentiate the system memory & flash memory in STM32MCUs, Whats the use of the both memory?Where we need to store the user code & where we need to store the customized setting?How to store FAT(File Allocation Table)?How ...

Sprak.11 by Associate II
  • 4628 Views
  • 2 replies
  • 0 kudos

Resolved! Locate the STM32F405RGT6 HAL_User_Manual

I cannot find the ??-> STM32F405Rx_User_Manual <-?? in the STM32F4xx_HAL_Driver package in the STM32Cube_FW_F4_V1.24.2 in my repository. Is it available? Also I would like one for the STM32F4 Discovery's 407VGT6 MCU as well, but the 405RGT6 would suf...

JSmit.22 by Associate
  • 892 Views
  • 2 replies
  • 0 kudos

Can STM32 set it self to bootloader mode thru software

I am trying to get STM32 to set it self bootloader mode.One processor that I am trying to do it with is stm32f070rb and the second is stm32f070x6.I send command to each of them, and in their program I set RX Callback to handle this command.here is ex...

0690X00000BvqOcQAJ.jpg 0690X00000BvqOwQAJ.jpg 0690X00000BvqPGQAZ.jpg
DKubi by Associate II
  • 1411 Views
  • 5 replies
  • 0 kudos

STM32L4x3 USB Device connections

Hello,I am developing a product with the STM32L443 and I want to include a USB connection manly for debug via COM port. The product is self powered therefore I don't need to use VBUS to power the device or recharge a battery. I have couple of questio...

FR_INT_ERR with FATFS (dir_sdi) function

I am using STM32L1 MCU with SPI communication to SD cardI am using the FATFS library f_mount, f_mkfs and f_getfree are going fine but f_open returns an FR_INT_ERRDid anyone face this issue before, or have an idea on how to fix it?

TKou by Associate II
  • 2652 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F103 USB-CDC does not work

I am trying to communicate my Maple Mini clone board with PC without using a USART hardware. I've configured MCU with STM32Cube IDE which has STM32CubeMX in it. I've enabled USB hardware, set it to FS, set FS mode to CDC. After I flashed that firmwar...

Nuppo by Associate II
  • 3892 Views
  • 7 replies
  • 0 kudos