STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading USB flash drive on Nucelo-H743ZI2

Hi,I am trying to read a USB flash drive via USB OTG function on a Nucleo-H743ZI2 board.I am using STM32CubeIDE to generate most of the code automatically and following the example of FatFS_uSD_Standalone comes with the STM32 firmware. The example wa...

0693W000001sxdYQAQ.png 0693W000001sxeWQAQ.jpg
JZhan.9 by Associate II
  • 915 Views
  • 0 replies
  • 1 kudos

Ethernet frame problem

Hello siri am getting error hereif(((heth->RxDesc->Status & ETH_DMARXDESC_OWN) == (uint32_t)RESET)) in stm32f7xx_hal_eth.c file.where value of status never changed so I am getting no frame in reading of ethernet frameDipak Garasiya

Does CubeMX -F4x freeRTOS/LWIP actually work?

I created a project for the Nucleo-F207 board using FreeRTOS and LWIP that worked. But when I tried to re-create the same project for the -F429 it did NOT work. [However the -F207 binary did work when loaded on the -F429 board.] On the -F429, DHCP...

STM32F407 USB related questions

Hi! I have several questions regarding standard USB host implementation.1) Host mode: File "stm32f4xx_ll_usb.c", function "USB_HC_StartXfer" there is a piece of codeif (dma == 0U) /* Slave mode */ { if ((hc->ep_is_in == 0U) && (hc->xfer_len > 0...

VYare by Associate II
  • 4121 Views
  • 8 replies
  • 0 kudos

Problems with STM32L552CCU USB-VCP

I'm unable to get the USB peripheral to work on this chip. For some reason even the USB_FS_IRQn won't fire. This chip has no external vbus detection or VDDUSB. I checked PWR CR2 USV is 1 and I can have the host detect the device by controlling the us...

VBarn by Associate
  • 1165 Views
  • 1 replies
  • 0 kudos