STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-H7S3L8 ST-ZIO mapping

Is there any mapping document like this one on the H7S3L8 as there is for the H743ZI-B01?I only find this document:https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/26/49/90/2e/33/0d/4a/da/DM00244518/files/DM00244518.pdf/j...

htxy by Associate III
  • 506 Views
  • 1 replies
  • 1 kudos

Resolved! STLink V3MINIE no target voltage

I have the STLink V3MINIE. When connected to the PC the red power LED is on. But I can't program any device because there is not target voltage. ST Prog (v2.17) shows Target voltage 0.00 VHow can I fix this? Is there a jumper or solder connection mis...

Screenshot 2024-07-30 093547.jpg
Seba52 by Associate II
  • 8752 Views
  • 14 replies
  • 1 kudos

STLINK-V3MODS RTS/CTS -> RTS/DTR ?

Hello world :)I found STLINK-V3MODS extremely useful for automation testing (NuttX RTOS). I have ~50 different boards, some of them does not have on-board flashing capability, thus either JTAG/SWD or UART needs to be used.Most of the boards that use ...

CeDeROM by Associate III
  • 1085 Views
  • 3 replies
  • 2 kudos

Resolved! SPI on STM32G031

I'm attempting to configure SPI1 on an STM32G031.   However I must be missing something because there is no data being output.   I am trying setup SPI to transmit 16 bits at a time.  Any suggestions would be appreciated.   I'm running the uC at 64Mhz...

Resolved! SWO only works at 16MHz with STLINK-V3PWR

SWV 16MHz, SYSCLK 16Mhz = logging worksSWV 16MHz, SYSCLK 25Mhz = logs gibberish (expected)SWV 25MHz, SYSCLK 25Mhz = logs nothing at allSWV 48MHz, SYSCLK 48Mhz = logs nothing at allWhy would this be?It works with HSI 16MHz, so my wiring and configurat...

NateS by Associate III
  • 4281 Views
  • 8 replies
  • 4 kudos

STSW-LINK007 on FreeBSD

Hello world :)Trying to upgrade firmware on series of STLINK-V3MODS on FreeBSD, downloaded 3.16.9 package from [1], after running:java -jar STLinkUpgrade.jarI got error message "Platform not supported (freebsd)".Would it be possible to add support fo...

CeDeROM by Associate III
  • 1341 Views
  • 6 replies
  • 0 kudos