User Activity

Dear ST community,I noticed that the CRC API is forcing the input buffer to be aligned 32 bits, which can be understood in order to be generic, but in the majority of the case we have a byte buffer which could be stored in unaligned in the memory or ...
Dear community,I'm not a big expert of USB and I have a solution based on STM32C0 and I would like to extend it to use USB, STM32C071 is the prefect candidate, but for my big surprise the USB stack is based on Azure RTOS, this is kind of killer for u...
Dear community,I have a nucleo board NUCLEO-G071RB and I would like to use the Build-In USB in the STM32G071, is there a shield or an expansion board compatible with this nucleo board, that allow me to access to the USBThank you in advance.Best regar...
Dear support team,I download recently the last release of Stm32cubeF4 v1.28 and I have the MDK V5.38 installed in my machine, so normally I was expecting that examples will build out of the box but it's not the case.It looks like the project example ...
Kudos from
Kudos given to