cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-DISCO built-in display issue

junseok3607
Associate

I am working on a project using the built-in LCD display of the STM32H747I-DISCO board. However, the display output shows unintended thin lines and color distortions, appearing as if the colors are breaking. I am unsure whether this issue is caused by a hardware defect in the display itself or a misconfiguration in the IOC settings and debugging process.

 

To troubleshoot, I ran the TouchGFX game example without any modifications, but the same issue persists. I would appreciate any insights or suggestions on how to resolve this.....

 

IMG_8433C6A6F16A-1.jpegIMG_5854.jpeg

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
AScha.3
Super User

If the not working line is on constant position, if running different software/programs, it probably a hardware problem.

The TFT protective foil shows, it had already experienced a lot of treatment/use...

So pressing a little on the outer TFT area /contact/connectors -  are any changes on the display errors?

(most times this is a lost/bad contact to a line )

If you feel a post has answered your question, please click "Accept as Solution".
mƎALLEm
ST Employee

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.