STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with ST Link Update

Posted on April 03, 2017 at 18:14Hello,When i connect my STM 32F401RE to the STM32 ST-Link Utility and then try to update the firmware, it says that Version V2.J27.M15 is the latest.When i do the same with ST-Link Upgrade (stswlink007 from st.com), ...

Programming an external flash

Posted on March 17, 2017 at 13:39Hi I'm trying program an external flash with the ST-Link Uility. I made a custom External Loader based on STM32F429ZI and the memory to program is a NOR flash S29GL128S (http://www.cypress.com/file/177976/download). ...

Nickjmas by Associate III
  • 2266 Views
  • 7 replies
  • 0 kudos

JTAG connection with STM32F7

Posted on March 03, 2017 at 16:25I'm using a STM32F7 MCU with a JTAG connection (4-pins used). The schematic is attached. It uses the http://www.keil.com/support/man/docs/ulinkpro/ulinkpro_jtag_10pin_swm.gif, and it's connected to a ST-LINK using th...

NPOR in STM32F098

Posted on February 19, 2017 at 17:17Hello there,I am working with STM32F098 mcu, it has NPOR pin. Reading the documentation I understood that I have to externally pull this pin low until a stable VCC will be present. When it is present, I have to le...

0690X0000060MqGQAU.jpg

Creating a st-link programmer

Posted on February 17, 2017 at 10:30Hi,I would like to use a STM32F103 micro as a st-link programmer on my board to program or debug another micro using USB (like the one on STM32F4 Discovery board). Is it possible to download the st-link firmware t...