cancel
Showing results for 
Search instead for 
Did you mean: 

STLink utility : ''No STLink detected''

maxzor
Associate II
Posted on August 16, 2016 at 17:32

Hello, I have trouble setting a STLink, been looking alone for days but still have no solution. The sensitive points in my opinion will be underlined.

I have a hard time posting photos here because of the max file size.

I am using a STLink sawn-off from a Nucleo-L053R8 board, MB1136 revC.

I want to access a STM32F427 custom board.

The STLink and custom board both boot and are recognized in Windows device manager as STLink debug/STLink virtual COM port and serial USB respectively.

 

When both boards are powered via USB, trying to connect in STLink utility issues a pop-up ''No STLink detected''.

The wiring used is SWCLK, GND and SWDIO.

(I assumed that the closest pin to the CN12 jumper, on the CN4 connector, was the 3.3V target.)

I removed CN2 jumpers.

I installed ST-Link/V2 v3.9.0 and since repaired it.

It installed drivers. Trying to get a connection, 

afterward I replaced drivers with ones from Zadig,

 I then removed drivers from the device manager, and reinstalled the drivers from STSW-LINK009

amd64.exe.

 

I still have not managed to connect with st link utility once, even when I try to connect back to the nucleo chip as described in UM1724...

As I understood that Clive1 does a huge job helping others, I will thank him a lot, or anyone that would chime in, for their time spent helping here.

Maxime

#stlink
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
maxzor
Associate II
Posted on August 16, 2016 at 19:33

Problem resolved... ''Ccleaned'' registry. :o