STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

cannot connect to stm32f4

Posted on November 11, 2012 at 14:36 The first problem I got, was when using debugger in IAR: Fatal error: ST-Link Connection error. Then I tried to erase flash with stm32 st-link utility, but I get an error: No STLink detected. An...

blaz by Associate
  • 1831 Views
  • 3 replies
  • 0 kudos

ST-Link Connection Error Using SWD

Posted on October 31, 2012 at 15:49Hi all, I used STM32F4Discovery successfully using SWD and IAR to develop my application. Today I got my boards, they have STM32F405RG on them (the Discovery has the 407). I tried to connect to the board using Segg...

igal by Associate II
  • 1620 Views
  • 1 replies
  • 0 kudos

STM32 ST-Link Utility memory leak

Posted on November 01, 2012 at 06:41hi I'm using ST-LINK utility version 2.4.0 with STLinkUSBDriverdll V4.2.3.0 and ST-Link_CLI V1.4.0. I'm using Win 7 x64. I'm using a ST-Link V2 If I use it in ''automatic mode'' it seems to leak memory at an amazi...

peterm by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

Timeout during flash programming

Posted on June 10, 2012 at 19:46Hello! Hope you can help me to fix my problem.St-Link didnt see STM32F4 Discovery, but I've tried[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/DispForm.aspx?ID=1944&RootFolder=/public/STe2ecommunities/m...

timon1994 by Associate II
  • 6764 Views
  • 14 replies
  • 0 kudos

STM32vldiscovery and ST-LINK/V2

Posted on October 03, 2012 at 11:42I believe the original board only supported V1 which use the MSD SCSI transport layer for communications, where as the V2 uses direct USB end points.So is it possible to flash a STM32vldiscovery board to support ST...

OpenOCD and stlink-v2

Posted on August 28, 2012 at 09:03 I am trying to get OpenOCD to work with my STM32F4Discovery board and I get the following error: fabio@fs-1:~/workspace/stm32_code/test$ openocd -d 3 -f ./openocd.cfg Open On-Chip Debugger 0.6.0-rc1-...

usafape by Associate II
  • 9005 Views
  • 4 replies
  • 0 kudos

openocd

Posted on May 03, 2012 at 13:22 Hi all, i want to configure OpenOCD for Stlink(embedded on stm32vld board)... but after building and starting openocd i've got this output: openocd -f /usr/local/share/openocd/scripts/in...