cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f09 command line programming issue

JKucz.1585
Associate II

issue-when programming using the Command line utility it indicates success but the unit does not boot.  when programming from the GUI the unit powers up correctly.  I used the same command line on an st32f07 without issue.  Here is the command line.​  start /B/wait st-link_cli.exe -c SWD UR -ME -P c:\RF6_RP_FAC_1.5.bin 0x8000000.  Am I missing a setting/command?  I attached a screen shot of the firmware in the stlink programming utility

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0