STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Nucleo-H743ZI2 VCP Port / STLINKV3

HiI am currently evaluating the STM32H7 family on a NUCLEO-H743ZI2 board. I am having troubles with the UART. I checked the schematics for said board and it shows that the STLINKV3 on that board is connected to USART3 on the STM32H743. So I created a...

Thomas L. by Associate III
  • 3917 Views
  • 8 replies
  • 0 kudos

What does it mean the data called REvision ID? and It is related with the package info Revision code?

When we use STm32 ST link Utility software to read STM32F405ZGT6 it shows device data called Revision ID, what does it mean? and is it related with the mark located at the IC package called Revision Code?I´m asking cause we are seeing diferent inform...

GRese.1 by Associate
  • 2355 Views
  • 2 replies
  • 0 kudos

Hi,I am using STM32L431CCT6 MCU in my design. I have space limitation on my PCB and did not place pull up/pull down resistors on unused pins. Is there a problem? What is the recommendation here?

 My boot up time is about 30mSec. I would like to know how the pins behave during boot up. Does it behave as high impedance i/p or as o/p sourcing/sinking current? In my design I am shorting two IO pins. Is there a chance during boot up one can sourc...

SG.13 by Associate
  • 1090 Views
  • 1 replies
  • 0 kudos

STM32F777 1.125 Volt on VCAP

Is this a normal reading?Havent installed ALL caps yet. I think I had bad contatc between SWCLK and connector, could this have caused it not to be recognized by cubeprogrammer?I had a F2 with 1.188 volt wich I could program, communicate with via prog...