STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F777 1.125 Volt on VCAP

Is this a normal reading?Havent installed ALL caps yet. I think I had bad contatc between SWCLK and connector, could this have caused it not to be recognized by cubeprogrammer?I had a F2 with 1.188 volt wich I could program, communicate with via prog...

Resolved! Downgrading firmware?

I'm trying to downgrade a board to V2J27M15 and I read that you can do that using older version of ST-Link Utility, but I can't find where to download ST-Link Utility 2.3.30. Does anybody know? Thanks.

AMaca.1 by Associate
  • 1996 Views
  • 3 replies
  • 0 kudos

Can the ST-LINKv3 interface on the DISCO board be used with IAR Workbench to run workbench in simultaneous dual-core debug mode ( master/slave project constructs )?

I have seen simultaneous or synchronous dual-core debugging within Workbench using the I-Jet from IAR, and I believe the DISCO board has an interface for connecting an I-Jet to; however, I'm wondering why the ST-LINKv3 can't do it, as it supports sha...

Bug in STM32L432KC Nucleo resources

Refer to this download page.In package: en.nucleo-32pins_bom.zipEverywhere in the document, the wrong uC is mentioned (L412KB)In package: en.nucleo-32pins_sch.zipThe options for the external oscillator are not shown for STM32L432 (see image)It seems,...

0690X00000AtR6BQAV.png