Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, I have about half year experience now with STM32H750 hardware, and all working very nice now. Up to now I always had used Revsion Y chips.Now on the last order we got Revision V chips (LQFP100 housing, chip marking line 1: "STM32H750", line 2: "V...
Hi.I bought STM32F446 Sensor board ( Mezzanine Board ) .but I don't know how this device use.I use an IAR.If I connect Micro usb connector and download code, It shows me a fatal error message (ST Link, No device found).I found to standalone mode at...
When the device is connected to the ST_LINK, after firmware upload, it works perfectly fine. When I remove the ST_Link and then turn OFF and ON my device, it does not work, unless I initiate a hard reset.Also, the device works fine when I chose the i...
I had to replace this exact board already because the overcurrent LED came on and bricked my device the first time... now this new board will not enumerate as a device on any of my computers. I haven't had the opportunity to flash any code yet. The...
As this is a prerequisite to installing CubeIDE 1.1.0 one can not install correctly on Mac OS Catalina.Do we have an ETA for a fix this this problem.Download site has version 1.1.1. available for download, which is incompatible with Catalina./S
The schematics provided in the ST site for STM32H743-EVAL(MB1063-B02 Board Schematic) only contain LCD board information. Path: https://www.st.com/en/evaluation-tools/stm32h753i-eval.html#re Could you please provide the actual schematics for the same...
trying to blink the LD2 on PA5. Getting following error. Please help in resolving.STLINK is installed and showing in Device manager
External ST-LINK/V2 programmer/debugger with B-L072Z-LRWAN1 Discovery kitHi,I have bought:1)a B-L072Z-LRWAN1 Discovery kit (with on-board ST-LINK/V2-1 programmer/debugger)2)a separate ST-LINK/V2 programmer/debugger.I have downloaded and installed on ...
Hi, I'm using STM32L412RBT, LQFP64pin. As the attached schematic, we are using some GPIO's as BTN inputs. But, unfortunately, the GPIO got damaged very easily without special reason. The pin voltage stuck at 1.0 ~ 1.7V when the button is not presse...