cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link-Server incompatible with MacOS Catalina

SChri.1795
Associate II

As this is a prerequisite to installing CubeIDE 1.1.0 one can not install correctly on Mac OS Catalina.

Do we have an ETA for a fix this this problem.

Download site has version 1.1.1. available for download, which is incompatible with Catalina.

/S

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Ziyadak
Associate

UP

NJosh.1261
Associate

Tried with the recent version, 1.2.0. Yet without any luck!

ozcan
Associate II

Any reply from ST?

SChri.1795
Associate II

Hey ST,

Can we have an ETA for a new release of the STLink server. The STM32CubeIDE is currently only available as version 1.0.2 for MacOS.

And the STLinkServer can not be installed under Catalina.

All that is required here is to compile the App as a 64 bit app instead of the current 32 bit app. Should be doable in a rather short amount of time.

/S

THUER.1
Associate

Any update on this issue?

Please ST update the driver!

Best regards

BPass.1
Associate

Up !

An update will be really welcome now.

We have been promised a working delivery for the next release of CubeIDE from the team that handles this error and it's set as a blocker. So my guess is that it will be fixed in the next release.

ATulg.1
Associate II

Up!