STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! If you change the package

Thank you for helping.When changing from STM32F769NIH6 to STM32F769BIT6That is, when changing from BGA to LQFPI think the software can be used as it is.Is this perception correct?Thank you.

Ebun.1 by Senior
  • 1091 Views
  • 2 replies
  • 0 kudos

Resolved! My on board ST link V3 cannot work?

The development board is STM32H757I-EVAL which has a ST link V3 on it,but after I download my program (just once) and update the firmware, it cannnot work correctly.Here is the situation when I try to debug it:

0693W000002liNfQAI.png
RZHU.1 by Associate III
  • 1113 Views
  • 2 replies
  • 0 kudos

STLink-V2 Issue

I am having trouble communicating with a STM32F042K6T6 microcontroller (on a custom soldered board) via a ST-LINK V2. Whenever I try to connect I receive the error: “Cannot connect to target!�? The STLink V2 does register and I can see it in the soft...

JReas.1 by Associate
  • 1979 Views
  • 4 replies
  • 0 kudos

Using STLink V2 with openocd sometimes persists HW breakpoints. Is there a quicker way to clear them other than disconnecting the STLink V2 for an extended period of time.

Every once in a while when remote debugging I wind up with not being able to set HW breakpoints. There's no clear indication of when this will happen, and I'm typically only setting a single break point. If I disconnect the USB to the STLink V2 fo...

BBick.1 by Associate II
  • 812 Views
  • 0 replies
  • 1 kudos

Unable to debug with STM32CubeIDE after upgrading stlink firmware to V2.36.S7 version

Hi there,I am using STM32CubeIDE 1.3.0 with STM32L152x MCUs. When using ST-Link GDB Server, STM32CubeIDE insists on updating Stlink firmware to the latest version (Now is V2.36.S7). After that I get the following errors:ST-LINK SN : 49FF7606837056521...