Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, i tried connecting the board to my pc but it just says that the device is unrecognized. Ive installed the drivers provided by ST but it just doesnt want to connect anyway.Would anyone know how to rectify this? thanks.
UM2569 says:"In STM32H7B3I-DK boards labeled A1945xxxx, the ISM43340-M4G-L44-10CF is loaded with the C3.5.2.6.STM.BETA4 version which allows a network scan only once. A new version of the ISM43340-M4G-L44-10CF firmware named C3.5.2.6.STM that fixes t...
I configured IAR EWARM for dual core debugging of an STM32H7 processor following instructions from one of ST's application notes (AN5286).When I do, I get the following warning repeated endlessly in the log window:"Tue May 26, 2020 10:13:04: SWO not ...
On the STM32F0Discovery, there's both an ST-Link chip and the main STM32F051R8T6 MCU.Is it possible to power up and use the STM32F051R8T6 without also bringing up the ST-Link?If so, how?Thanks in advance.
I have experience with several types of classic boards with STM32 microcontrollers (NUCLEO, Blue Pill...) that immediately connect with the stlink-v2 and st-info --probe command showing the characteristics of the controller and after that flashing is...
we are using two micro controller one is nucleo L4R5ZI Board with STlink on board can be used as independent programmer and 2nd is ARM9 . we want to use this ST link programmer to program a ARM9 processor. is it possible? is STLink support older ve...
I have recently purchased a NUCLEO-L031K6 dev board and when connecting it via USB ST-Link won't get recognized. I have 2 other st-link which work like a charm, so drivers are there (STM Discovery F0 and ST-Link V2). Any help? Is there any boot seque...
I'm looking to use the Arduino header on the STM32H7B3i-DK, however I am finding an inconsistency between what is defined in the Schematic and what is listed in the Users Manual.Example: For header C10 Pins 1 and 2: The schematic shows these mapp...
I have just recieved this circuit board and im trying to program it with an ST-LINK V2 however i keep getting the error "no stm32 target found" when trying to connect to it through SWD. Could someone help me?