cancel
Showing results for 
Search instead for 
Did you mean: 

Does someone know which are the VREF+ and VDD values in the STM32F429Idisco? In the schematics, it seems that VDD is 3V (but I see it only from the other device), and Vref is connected to Vdd via R58, so I don't understand which is its value. Thanks?

Hicss.2033
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
David SIORPAES
ST Employee

Hello,,

In STM32F429Idisco all voltages Vdd, VREF+, VDDA are set at 3V. Note that R58 is a zero ohm resistor.

View solution in original post

2 REPLIES 2
David SIORPAES
ST Employee

Hello,,

In STM32F429Idisco all voltages Vdd, VREF+, VDDA are set at 3V. Note that R58 is a zero ohm resistor.

Hicss.2033
Associate III

Thanks for your fast answer!!