STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Okay I have previously posted on this community and got great feedback. So I spent a while fixing my schematic for the STM32F722RET6. If someone could check my pin outs of VDD and VSS that would help a lot.

It's an ugly schematic I know. The reason It's so tight is because I'm planning on adding more components, like a gyroscope, barometer, etc. I am using the ST-links debugger. But I just need someone to help and check my VDD and VSS pinouts. Each VDD ...

JZipf.1 by Associate II
  • 2344 Views
  • 4 replies
  • 1 kudos

Resolved! STM32F7508-DK; MxCube; CN4, CN5, CN6 and CN7

HI, I am a beginner with STM32 but an old programmer. Bytw, my father was born in Crolles ! English is not my natural language.I bought a development kit. I downloaded Cube MX. I create a project for this DK. But in the pinout window I can see pins t...

MJean.3 by Associate III
  • 3677 Views
  • 6 replies
  • 1 kudos

STM32F411RE PCB Layout

Hi there,i finished my program and the schematic design of my prototype. Now i want to start with the PCB layout. Therefore i have some questions regarding the Supply & Oscillators. At the beginning i implemented the DFU for programming the STM32F4, ...

Resolved! Problem with connection STM32H745

I've made a mistake and programmed to STM32h745 dual core processor program which was created to STM32H743 with one core. Now I have a problem with connection and ST-Link doesn't recognize device. What can I do with that?I've also tried to supply boa...

DBrau.2 by Associate III
  • 2576 Views
  • 4 replies
  • 0 kudos

MB1440 stlink -v3 board

Hi!I burned Stlink-V3 ic(u1-MB1440) while debugging.Maybe I entered the wrong power source.Can you tell me? What's the part number?  I couldn't find a part list or a circuit diagram of the mb1440 board.

kinhe.1 by Associate
  • 981 Views
  • 0 replies
  • 0 kudos