Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi all,I build a prototype board based on STM32G431KBT6 which need Virtual COM port and DFU firmware upload. In previous version of the prototype everything worked fine.Windows detected the board, I was able to send/receive commands over VCP and also...
Can desoldering and soldering to replace a capacitor which is part of an RC filter of an I/O pin cause that pin to develop an internal short to VCC? This problem has now happened on 14 PCBAs. Any insight would be gratly appreciated. Regardsik
Hello ,recently I upgraded to ST Link V3 and it works fine so far. Only one thing is annoying: I always get a double reset when uploading a new firmware from Cube IDE to my target. Console output is this:STMicroelectronics ST-LINK GDB server. Version...
Hi all:I have problems understanding the pull up/down situation with regards to 5V tolerance.I must admit that I have limited hardware knowledge, so please be gentle. I have searched and read a lot, but couldn't find a definitive answer yet.Say that ...
Hi everyonewe are developing simple iot gteway with reference of STM32F746 discovery board schematic.we have done assembling of controller sdram,norflash,rs232,usb2.0 sections one by one after testing with test codes.for ethernet we are using ksz8863...
Hi,I am quite new in this MCU world and I bougth a BluePill board (STM32F103C8T6) to start doing the basics and learn.At first I tried to use the IAR Embedded IDE to program the board but when I tried to debug the following error appears.Then I tried...
I'm using STM32H725IGK6. I come from Microchip PIC world.When pulling up 'BOOT0' with 10kΩ to VCC(3.3V) , I'm able to run my code on my custom designed board using STM32CUBEIDE.When I press RST or power cycle board, nothing runs. This is expected rig...
Hi,Is there, by any chance, a substitution for the white LED power supply for large display blacklight used in the STM32H45I-DISCO LCD schematic ?The product have 0 stock everywhere and will be available in 20 weeks. I can't wait that long to test my...
Hello.I want to write a program on M3 HiBot TITech Tiny Controller.This board uses STM32F205 VCT7.I connected ST-Link / v2 and the board by JTAG to write the program.1 (JTAG on the board) → 1 (TVCC: ST-Link / v2)3 → 5 (TDI)4 → 7 (TMS)5 → 9 (TCK)6 → 1...