Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello comrades...I have been using IAR 6.50 for a few years now with STM32F446VC 1-- pin uC and things have been working flawlessly. I also have more recently had a project using the STM32F334 controller and debugging just fine.Last week, all of a su...
After the update, I was unable to run or debug on my nucleo-l053r8 on MacOS Big Sur V11.4.
clock of SPI2_CLK pin effected to other GPIO as noise. i want to remove this noise. of course not effected because of board design i am already checked it.
Hi,I'm trying to make a STM32L100RC work as a CDC device as shown on this website : https://damogranlabs.com/2018/02/stm32-usb-cdc/Nevertheless, it didn't work for me, even when I used the exact same file shared on the website. The USB is always dete...
Hello,Im just starting with the nucleo board STM32L476RG using mac (10.13.6) and cube IDE 1.6.1. I also updated the firmware on the ST-link to the newest one when prompted.For the very first program I just wanted to make it blink to see if it works, ...
Is there any way to come around this? Or is this some "dirty trick" of the stupid "STM-Cube-Fan-Group" at STM to force all STM users into their stupid STM-Cube world?(If I try to connect Keil uVision 5.1 to the new Nucleo ARM G474 boards, the Keil Pr...
I am using STLINK V3 with the ISOL board, and using the supplied 10-core cable, going to this connector in my 32F417 targethttps://peter-ftp.co.uk/screenshots/202105072011602908.jpgOn the target connector, I have pins 3,5,7,9 grounded.Pins 2,4,6,10 g...
I have recently bought a stlink v3 mini and I have connected with STM32F103C8 (blue phill) board with SWIO, SWCLK, and Gnd. I tried to upload a blink program many times. But it says failed to start GDB sever and no device found on the target and I ...
HI!I made a custom board with STM32G474RC. Unfortunately the ST-Link V2 cannot connect to it. I have two pices of V2. (Bought from local store but probably clones.). This is the message I get: "No STM32 target found!" Tried it with CubeProgrammer, U...
Dear ST expert,STM32G474 serials are very good option on digital power control, and I see the WLCSP81 package is pretty small(only 4mmx4mm). I plan to use WLCSP81 package on 1/4 bick power module which is 12 layers and the topology is Hard Switch Fu...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.