cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to hold device in reset using ST-Link V2/V3?

JFOLE.1
Associate II

I am trying to load into external flash but while doing this I need to have MCU held in reset.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

You can connect to the chip with stm32cubeprogrammer which will effectively prevent it from running your program. There is also the "connect under reset" option, but I'm not sure if it holds NRST low or just toggles it momentarily.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

You can connect to the chip with stm32cubeprogrammer which will effectively prevent it from running your program. There is also the "connect under reset" option, but I'm not sure if it holds NRST low or just toggles it momentarily.

If you feel a post has answered your question, please click "Accept as Solution".