Skip to main content
ksamy.1
Associate
September 16, 2020
Question

NUCLEO-H745 + ST-Link Utility = Can not connect to target

  • September 16, 2020
  • 16 replies
  • 3900 views

We tried our custom board that has STM32H745XI through ST-link V2 with updated firmware. Initially in boot mode the board connects and we were able to read flash. Then after some time the SWD connection is lost.

It is not even able to debug the application. We measured the power supply on CRO and also connectivity with the MCU. We connected SWDIO,SWCLK and ground pins with the stlink.

This topic has been closed for replies.

16 replies

Uwe Bonnes
Chief
September 16, 2020

Does anything eventually remap SWJ pins? Does the application enter Sleep?

ksamy.1
ksamy.1Author
Associate
September 16, 2020

Application is also not getting loaded at first.so that may not be the issue.

Tesla DeLorean
Guru
September 16, 2020

I'd have thought the NUCLEO-H745ZI-Q would use an ST-LINK/V3

The H7 is very sensitive to the LDO/SMPS and VOS settings in your configuration code. Low power mode and WFI can drop the debug connection due to the circuits involved being turned off. Check also if you change configuration of the PA13/PA14 pins.

When you get invalid settings you need to power cycle the board with BOOT0 High, until you can connect with STM32 Cube Programmer, and then erase the errant code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
September 16, 2020

Check components and voltages on VCAP pins

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ksamy.1
ksamy.1Author
Associate
September 22, 2020

The voltage at Vcap is 1.005V and SDC voltge is 1.2V

Uwe Bonnes
Chief
September 16, 2020

The asker mentions Nucleo and Custom. I supposed he means custom board and StlinkV2.

Tesla DeLorean
Guru
September 16, 2020

Trying to decide if the NUCLEO is just a distraction..

Not really any familiarity with the custom board, potentially design or manufacturing issues there. Not clear what board bring-up checklist items have been met. Would have connected the NRST and SWO too. External ST-LINK/V2 needs to see target voltage.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ksamy.1
ksamy.1Author
Associate
September 22, 2020

The CN5 connector on Nucleo-H745ZI is SWD port. I have disconnected the on-board MCU(STM32H745ZI) and connected my custom board at this port so that it can communicate with SLink, but i receive message STM32 target not found even though correct voltages measured at VCAP(1.005V) and 1.2V at SDC

ksamy.1
ksamy.1Author
Associate
September 17, 2020

Today i connected the custom board with ST-link/V3. Error "STM32 target not found error" message received.

Measured Voltages: VDD_MCU=3.3V, VDD_LDO=3.3V, V_core=1.005V.

SWD Clk and SWD_IO signal measured on CRO and able to see clock and data. Any further suggestion what could go wrong?

ksamy.1
ksamy.1Author
Associate
September 17, 2020

image of error for reference

Uwe Bonnes
Chief
September 17, 2020

When going off-board, a speed of 24 MHz may be detrimental. Try with lower speed.

ksamy.1
ksamy.1Author
Associate
September 17, 2020

After removing level translator that is used in nucleo board (in swdio and swo lines) and keeping the on-board MCU supply jumpers off, Now we are able to connect the STM32H745XI custom board in boot mode and erase flash successfully. However, we are not able to load firmware or debug in normal boot mode. Any suggestion on this.

Tesla DeLorean
Guru
September 17, 2020

Need to cycle power after first code load.

Check option byte settings.

I​ would probably start by getting a UART running so I could report on internal state. The work on getting HSE and PLL up.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ksamy.1
ksamy.1Author
Associate
September 22, 2020

how to connect stlink v3 of nucleo-h745zi to external stm32H745 custom board?

ksamy.1
ksamy.1Author
Associate
September 22, 2020

Finally resolved the problem: if we want to connect the nucleo-H745ZI stlinkV3 to external custom board (STM32H745XI) using CN5, then we need to remove few components that disconnects vdd, smps and ldo supply from main mcu U14(144pins).

Thanks everyone who replied to my queries.