STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F1-Error debugger

 I run into this problem every time I debug. No matter what I did I couldn't fix it. Even though I selected Debug configuration>Debugger>ST-LINK(OPENOCD) and Reset mode>software system reset it still works. I made a chip earese from the ST-LINK UTILI...

0693W00000GWkJvQAL.png
Hg.1 by Associate
  • 1230 Views
  • 2 replies
  • 0 kudos

STMCubeProgrammer does not program STM32L55

Hello, I am working on NUCLEO-L552ZE board which has STM32L55 Cortex M33 MCU.I can program the device using Keil IDE using ST-Link Debugger option. But I would like to program the device using ST-Link Utility or STMCubeProgrammer. ST-Link Utility can...

Murat by Associate III
  • 1544 Views
  • 2 replies
  • 0 kudos

stlink v3 mini overheat.

I have a stlink v3 mini and it gets very hot only when connecting to the usb port without connecting anything to the debbuger terminals, even so I connect it to the card to program and program without problems, but after a few minutes, it sends conne...

JMora.5 by Associate II
  • 2839 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G030F6 OSC_EN

Hello,I am using STM32G030F6, use HSE, but when I set the system clock, PA14 change to OSC_IN but while PA15 change to OSC_EN, and I can't find any specification of this definition, can I use it as OSC_OUT?

0693W00000GW2fsQAD.png
Qwang.2 by Associate II
  • 4747 Views
  • 9 replies
  • 1 kudos

STLink v3 Mods not flashing STM32H7 MCU

We have a STLink v3 Mods which is not capable of programming any STM32H7 MCU. The programmer works fine with G4s, F3s, F4s and L4s. Using the STM32Cube Programmer and 4kHz as a connection speed works fine for reading and writing. Higher speeds do not...

Ltech.1 by Associate
  • 1540 Views
  • 2 replies
  • 1 kudos