STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't get my controller in Low Power mode

Hi,My controller still consumes 360µA in STOP mode, i can't figure out why.Maybe one of the inputs/outputs that leaks current?I have this IO setup the moment i execute STOPPA0-PA5 = External interrups up down edgle no pull up of downPA6 = ADC inputPA...

0693W00000GYEMNQA5.png
sde c.1 by Senior II
  • 1050 Views
  • 3 replies
  • 0 kudos

STM32 programming using ST link V2.

Hi, We are using STM32F407VG MCU for one of the project and for programming we are using ST link V2. The MCU has SWD pinout, when we try to connect the MCU using STM32cube programmer we are getting the below errors,ST-LINK error (DEV_USB_COMM_ERR)Err...

SA.3 by Associate II
  • 5021 Views
  • 7 replies
  • 0 kudos

How Debug Works in ST-Link?

Hello, I'm researching the mechanisms of debugging in STM32F407 MCU using several debug probes. I previously used J-Link and I could see the details of the breakpoints in the FPB unit, but when I switched to ST-Link I couldn't see the details of the ...

MLeff.1 by Associate
  • 1037 Views
  • 1 replies
  • 0 kudos

Resolved! How GPIO speed is implemented on hardware lvl

Hello! I need to know how GPIO speed control is implemented. Unfortunately, no information was found in the documentation. All that is known is that the signal front is growing faster or slower, but why? I need some hardware schematic or diagram etc....

VKlim.1 by Associate
  • 1149 Views
  • 1 replies
  • 0 kudos

SWD DEBUG Communication STM32H7 ISSUE

Hi everybody,I'm facing to a strange issue linked to debug using SWD interface with my STLINK V3 for my µC STM32H7. I can download firmware .bin using TeraTerm (using UART RS232).However I'm unable to communicate using STM32Cube IDE in debug mode or ...

geek12 by Associate II
  • 6862 Views
  • 11 replies
  • 0 kudos