User Activity

Hi guys. I am using STM32G431KBT MCU. I am using 2 MCU (master / slave) and they communicate via canbus. Canbus is working good but canbus filter is not working. Master canbus address is 0x200 ans slave address is 0x101. I changing master ID (0x150) ...
Hi guys.I've been trying to work hardware video decoding for a few days but it doesn't work. Latest situation is as follows:I think I made all the settings correctly.1- Enable JPEG.2- Enable MDMA channel 6 and 7 for JPEG output fifo - input fifo.3- E...
Hi.I am using SDRAM, OctoSPI and 24bit RGB888 TFT screen. Project is working normally with another widgets (button, shape, text area, image etc.). Now i want to use video decoding and video widget. I made the necessary cubemx settings by reading the ...
Hi.I am using STM32H7B3LIHQ MCU, MX25LM51245GXDI00 OSPI flash, IS42S32800J-6BLI SDRAM and 24bit TFT screen. I used the schematic of the STM32H7B3I-EVAL (MB1331) board when creating the scheme. I wrote programs for FMC, OctoSPI and LTDC peripherals us...
Hi.I am using STM32H7B3LIH MCU and Newhaven "NHD-4.3-800480CF-ASXP" TFT. I completed all the configuration according to the instructions in AN4861. I am trying to show an 800x480 image on the screen using framebuffer. I use "LCD image converter" to c...
Kudos from
Kudos given to