Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi All,Does anyone have the circuit diagram (schematic) for this board?Basically (and I have posted about this before, without any conclusion) I have several boards which work perfectly (sw download and SWD debug) via the big 20-way CN2, but are unre...
my goal is to use this board in [-40°C +85°C] climatic chamber.Regards:)Oliver
I'm using an ST-Link/V2-ISOL and installed the drivers (stsw-link009_v2.0.2) and ST-Link utility but I keep getting the "Target, detection failed" error in the Utility. Same result in the STM32 Cube Programmer. How can I fix this issue? I am using 64...
We were using STM32H730VB to drive a LED display in our project. Pins 51 - 64 drive the LED display, Pin 30 controls the display power, and pins 24 - 25 act as the USART. We use CubeProgrammer to download the firmware.This worked well and with no is...
OK, OK, OK, this is a REALLY dumb question but for the life of me I cannot find out WHERE you turn your hard-earned project with all its bells and whistles into a RELEASED file to download into the proc??!!??I know this will come back as an easy thin...
Hi,I am using STM32F746NG discovery board. I try to setup 60 micro second delay. With ST-Link debugger, the 60micro second delay is fine. But when I cycle the power, the firmware does not run.When I comment out the delay function DWT_Delay_us(), firm...
I am planning to automate the Circuit Verification for inhouse designed&assembled electronics, this is my rudimentary idea:(For me ,the blurry concepts because lack of experience are the Tensorflow and database parts) Does anyone have experience/idea...
Hello,I currently working on a projet where I've ordered custom PCB with STM32F030C8T6 already installed by JLCPCB but I can't communicate with them.I've connected the STM32 with 3.3V and ground and then I output the SWD and SWCLK pins. I connect the...