STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I bought a STM32F100RB Discovery board and didn't realize at the time that it only comes with the ST-LINK V1. Is there a way to update the STM32F103C8 that is used for programming and debugging to ST-Link 2.1?

I have done a bit a research already to try and figure out if I could do this. First thing I tried was to use the ST Link update tool but that just updated it to the newest ST Link V1 file. I also found this link https://visserslatijn.wordpress.com/2...

JWire.1 by Associate III
  • 4700 Views
  • 8 replies
  • 0 kudos

STM32G4 pin shortage issue

Hi,We are planing to use stm32g4 higher end micro controller 128 pins(107 GPIO). We had faced issue for pin shortage.We want to know JTAG, Oscillator we can use as multi functionality (Ex - Debug as well as GPIO or etc...) functionality ?Pins:PA15 - ...

VDhev.1 by Associate II
  • 2180 Views
  • 3 replies
  • 0 kudos

What are the BOR levels for STM32G030 ?

Hello!When I connect to STM32G030 with the ST-Link programmer in the Options bytes tab, I can adjust the BOR levels (level 1-4 F and R). These levels are not described in the datasheet (DS12991 Rev 3). What are these levels and where can I find their...

Akoli.2 by Associate III
  • 4023 Views
  • 1 replies
  • 0 kudos

Also, I heard "Pull-up resistors are not require because STM32F already have one." is that true? Please help me about it. I will be really appriciated.

 Hi everyone, I am confuse about I2C pull-up resistors. I use 4 I2C sensors. I am not sure is it true that pull-up resistors count. I use every sensors for pull-up resistors. If I use just one I2C port (I mean one port for all sensors) is it enough? 

0693W00000HncMpQAJ.png
AElma.1 by Associate II
  • 8143 Views
  • 5 replies
  • 1 kudos

STM32L073RZT6 hardly booting the firmware

Hello ST Community,I have a PCB designed according to the attached schematic.Recently, I have been struggling with the following awkward issues:1) The flashed firmware (via UART) doest not always start (2/10 attempts lead to successful code execution...

VMeto.1 by Associate II
  • 3986 Views
  • 6 replies
  • 0 kudos