Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I want to program my µC with the MB1440B board, but the STLINK doesn't find any target as soon as I plug in the MB1440B. Programming with the MB1441B alone works just fine. Do I need to change any jumper configuration? I didn't find any description i...
I have a number of full-speed USB-powered devices I'm working with. All use STMicro microcontrollers (a few different models, including STM32F205, L432, etc.). All of the different devices use the same USB circuitry (including the 1.5k internal pullu...
i am using nucleo-f429zzi. there is reset button (B2) is connected to NRST in mcu. Is it possible to use program to detect this button is clicked? Actually, I would like to stop some digital i/o when user presses this button to reset the system. It i...
/home/i/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammer: line 4: 3947 Aborted (core dumped) $DIR/jre/bin/java -Djdk.gtk.version=2 -jar $DIR/STM32CubeProgrammerLauncherthis is the output I get to the terminal ...
Hi,i have bought 3 pcs of STM32L053 Discovery kits and the user USB is working fine with preload demo, but the ST-LINK USB connects to PC as USB Composite Device even if i have download and install the last ST-Link drivers from st.com. I have tried d...
Hello everyone. What do you use as wifi module or ic in your pcb circuits, including stm32 processors. I don't like working with AT commands. I would like to work with SPI or SDIO interface if possible. Can you suggest a solution with libraries and s...
Colleagues, I made a PCB project that contains Ethernet, GPS and STM32F429. but there was a problem. that GPS actively loses satellites when Ethernet is connected. I use RTOS and LWIP. I don’t know how to explain this ... capacitors - filters, did no...