2021-02-15 2:02 AM
I have started:
2021-02-15 2:30 AM
The stand-alone ST-LINK/V2 does not provide a COM port
2021-02-15 4:52 AM
OK. Misunderstanding here.
Rephrase question: How do I make the ST-LINK/V2 ISOL work? No STM SW (or any SW) identifies the device, except the installed driver
I would really like to use the prifiler.
I have made contact between STMC Workbench and the STEVAL-ESC001V1 with a self built USB-COM port.
Again, how do I make the ST-LINK/V2 ISOL work? An how should it be connected?
Rgds
/Jon