STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer 2.10.1 Will not connect to ST-Link Nucleo (ST-Link V2/1) or Discovery ST-Link V3

Hi, I recently updated:CubeMX (6.5.0)CubeIDE (1.9.0)CubeProgrammer (2.10.0)I am having trouble with the Programmer not connecting to the targets either the Nucleo F411RE or the H7B3Li-DK. I have not tries any other types of boards.Pushing the refresh...

0693W00000Kclc8QAB.png 0693W00000KclcDQAR.png 0693W00000KclcSQAR.png

Hi, I designing a new design with STM32L471ZGJ6 MCU. I connected crystal osc S.N. ECS-.327-12.5-1210B-N-TR to PC14, PC15 pins

Hi,I designing a new design with STM32L471ZGJ6 MCU.I connected crystal osc S.N. ECS-.327-12.5-1210B-N-TR to PC14, PC15 pins in MCU.Is the value of the capacitors I connected correct? (see image below)Is the connection correct? Thanks,Mor

0693W00000KczQGQAZ.png
mgeda.1 by Associate
  • 891 Views
  • 2 replies
  • 0 kudos

Resolved! No ST-LINK detected - only in CubeIDE

Hey guys,I try to connect a NUCLEO-F429ZI board with STM32CubeIDE.I have first installed the latest version of the IDE on an Windows 10 machine with the ST-LINK USB drivers that are required. When I know try to run or debug a simple example project t...

Thieny by Associate II
  • 23174 Views
  • 9 replies
  • 2 kudos

STM32G030C8T6 GPIO distubs each others.

HI,I use the G0 serial​s firstly. I have welded 8 model machines,but I found some similar problems. For exampleOn the NO1 board, I used the pin PF1 be output.The problem is that the voltage of the MCU's reset pin is not High toVDD。So the mcu keeps r...

0693W00000Kcm9gQAB.png
doming by Associate II
  • 1763 Views
  • 3 replies
  • 0 kudos