cancel
Showing results for 
Search instead for 
Did you mean: 

What are the design criteria for Nucleo Oscillator?

ALisk.1
Associate II

What are the design criteria by which the oscillator for the Nucleo dev kits has been selected?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Cheapness? The BOM call out the exact part numbers if you want to know the ppm, temp range, and load capacitance..

There are literally dozens of "Nucleo" boards, including 32, 64 and 144-pin formats. Can you perhaps narrow the question a little?

There is an Application Note on Crystal selection, and component values.

The NUCLEO's include an ST-LINK/V2 connecting via USB, USB places accuracy expectations on the clocking.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee

Hello @ALisk.1​ and welcome to the STM32 Community,

I recommend you this AN2867 Application note Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs, it provides guidelines for the oscillator design. 

When your question is answered, please close this topic by choosing "Select as Best".

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
To be clearer:
Is there a specific reason that ST selected the NX3225GD for Nucleo 144pin?
Price?
Stability?
ESR?
Tolerance?
etc..
Thanks