STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0B1KET not "booting"

Hello, I designed and assembled a simple circuit around the STM32G0B1KET and after connecting my ST-link it does not seem to "boot". My circuit looks like this: Additionally, there is a red LED through a 330Ohm resistor connected to 3.3vI am poweri...

0693W00000Lx6SIQAZ.png 0693W00000Lx6TLQAZ.png

Resolved! 3.3V external power supply

Hi everyone, I need to power my F401RE with a 3.3V external power source. I read in the datasheet I need to connect the power source to the CN7 pin 12 or CN7 pin 16. Where do I connect GND signal apart from 3.3V signal?Also, from what I understood, I...

Problem with the nRST pin in a STM32L021K4

I already read this post with no success: https://community.st.com/s/question/0D50X00009Xka0fSAB/problem-with-the-nrst-pin-in-a-stm32f100cbt6I tried to design a simple board with a STM32L021K4 and to program it with a STLINK-v3 MINI. I got the follow...

LFIAC.1 by Associate II
  • 4267 Views
  • 5 replies
  • 0 kudos

Resolved! Internal RTC clock lag issue

I am using below componnet toolsMCU: STM32H7B3IIT6IDE: STM32CubeIDE Version: 1.9.0CRYSTAL: RT3215-32.768-12.5-TR ( 32.7680KHZ 12.5PF)I work with internal RTC. I will use for clock. But RTC clock behinds real clock. While the product is running, the l...